comment ## Set Precharge Command
setmem 0x00221000 0x92110200 32

comment ## Issue Precharge all Command
memory 0x08100000 +1 32          

comment ## Set AutoRefresh Command
setmem 0x00221000 0xA2110200 32 

comment ## Issue AutoRefresh Command
memory 0x08000000 +1 32         
memory 0x08000000 +1 32
memory 0x08000000 +1 32
memory 0x08000000 +1 32
memory 0x08000000 +1 32
memory 0x08000000 +1 32
memory 0x08000000 +1 32
memory 0x08000000 +1 32

comment ## Set Mode Register
setmem 0x00221000 0xB2110200 32

comment ## Issue Mode Register Command
comment Burst Length = 8
memory 0x08088C00 +1 32           

comment ## Set to Normal Mode
setmem 0x00221000 0x8211E267 32

ld "<insert path here>\Flash Loader J3 x16.new.axf"
lb "<insert path here>\FSL_MXSdevkitImage_Flash8MB_RTM.bin" 0x09000000

go

go